For Flexible Body analysis, does NX Motion support the Mode Acceleration
Method and does it include the option to add Residual Vectors?
Solution
Mode acceleration is not supported. The mode displacement method is used for
NX Motion Flex Body Simulation.
MBDEXPORT SCMOTION FLEXBODY=YES is only valid in a SOL 103 run. RESVEC is OFF
by default for the residual structure in SOL 103. Users will need to add the
RESVEC case control command to get residual vectors if desired.
Notes