Can't cut through some parts on drawing

2021-10-06T23:26:11Z

Summary


Details

In a Section view of an assembly, some components are not cut.

Solution

These components hold an attribute "SECTION-COMPONENT=NO", that's the reason.


Removing or changing the value for attribute SECTION_COMPONENT does not work for the existing 
Section view, nor for a newly created Section view from the same parent view, because the parent view 
stores that attribute information.
Once this attribute is removed or changed to YES, a new parent view has to be created, 
then a new Section view created from that new parent view.


For existing Section views that have components not being sectioned there's a quicker way to resolve it 
without recreating the parent view and Section view :


- Menu --> Edit --> View --> Section in View...
- Select View  --> Select the existing Section view
- Select Object --> Go to Assembly Navigator and select the component(s)
- Action  --> Set to "Make Sectioned"
- O.K.
- Update the section view(s).

Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 764SP1
Product: NX
Application: DRAFTING
Version: V10.0
Function: DRAWING/VIEW

Ref: 001-7936197

KB Article ID# PL8003009

Contents

SummaryDetails

Associated Components