Blends with sharp edges

2021-10-06T23:26:11Z

Summary


Details

Model shows Blends with sharp edges at the start and at the end of an Extrude.
When editing the "Extrude" feature and changing the values to something else than the current value, 
then the display is correct.

Solution

It's a visual issue in Modeling with the Shaded views, in Studio rendering mode, it looks correct.
When placing drawing views in Drafting, it's also O.K.


Visualization Preferences, tab "Faceting" and set the Resolution to "Fine", then the display is correct again.



Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 764SP1
Product: NX
Application: DESIGN
Version: V10.0
Function: FEATURE_MODEL

Ref: 001-7905653

KB Article ID# PL8003008

Contents

SummaryDetails

Associated Components