Details
Creating a note with leader line --> Choose settings - Line/Arrow - Arrow Line
There's no field to change the gap between text and leader.
Solution
Preferences - Drafting --> Dimension :
If Dimension "Text"->"Orientation and Location" is Orientation "Text Over Dimension Line", then "Text to Line Gap" is not present in the Settings.
Only if Dimension "Text"->"Orientation and Location" is anything else, then "Text to Line Gap" is present in the Settings.
Note : This was reported in 7398600 and is fixed in NX10.0.3 MP9 and NX11
Hardware/Software Configuration
Platform: INTL64
OS: window
OS Version: 764SP1
Product: NX
Application: DRAFTING
Version: V10.0
Function: ANNOTATION
Ref: 001-7866883