Generated Standard Parts are automatically 'Released'

2021-10-06T23:51:20Z

Summary


Details

Generated Standard Parts are automatically 'Released', which will prevent customer from changing them.
This was due to a change to previous Solid Edge versions.

Solution

For ST9 and ST10 the user needs to set a flag in the Registry:

1.  Open Registry Editor
2.  For ST9 navigate to HKEY_CURRENT_USER\SOFTWARE\Unigraphics Solutions\Standard Parts\Version 109
     For ST10 navigate to HKEY_CURRENT_USER\SOFTWARE\Unigraphics Solutions\Standard Parts\Version 110
3.  Create a new key as STRING, named "ReadOnlyFlag" and set the key to the required behavior:
 a. If the value is "True" then the "release status" is set to "OFF" and "read-only flag" is set to "ON".
 b. If the value is "False" or missing, then the "release status" is set to "ON" and "read only flag" is set to "OFF".  This is also default behavior, if the registry key does not exist.



Hardware/Software Configuration

Platform: INTEL
OS: window
OS Version: 764
Product: SOLID_EDGE
Application: EXTERNAL_APPS
Function: STANDARD_PARTS

Ref: 001-8998849

KB Article ID# PL8003003

Contents

SummaryDetails

Associated Components