NX Expanding subassembly with structure only shows an incorrect name for descriptive part name

2021-10-06T23:26:10Z
NX for Design

Summary


Details

When loading a structure-only assembly with 3 to 4 levels of subassemblies, 
the column of "Descriptive Part Name" is not displaying the complete name 
after expanding the structure.


(1) In Customer Defaults > Assembly > General > Miscellaneous tab, the 
"Structure Update on Expand" is OFF. 
(2) Load an assembly with 3 to 4 sub levels into NX using Structure Only load 
option. 
(3) Configure Assembly Navigator column to show "Descriptive Part Name" as 
first column and Object as second column. 
(4) Expand all levels of subassemblies. 
Notice the name shown under the Descriptive Part Name is not complete, also 
notice the Object column does show the correct completed name.


Is the display for Descriptive Part Name working as designed? 

Solution

The "Descriptive Part Name" uses cached values unless the part is loaded, so 
the behavior is as expected. Meanwhile, the "Object" column is Teamcenter-based 
information on all components, that's why they show complete information.

Notes and References





Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 2012_R2
Product: NX
Application: NXMANAGER
Version: V10.0.3
Function: ASSEMBLY_NAV

Ref: 001-9003883

KB Article ID# PL8002986

Contents

SummaryDetails

Associated Components

Teamcenter Integration for NX