SEEC: Cannot find a way to hide map properties in the CPD window.

2021-10-06T23:51:19Z

Summary


Details

Successfully mapped several properties but do not want all of them to show 
in the CPD window. How can you hide these properties? 



Solution

The CPD columns are individually controlled via the Format Columns option in 
the Common Properties Dialog (CPD). If the column has a check box then it can 
be turned off from view.


These settings are written into the default location, 
%APPDATA%\Roaming\Unigraphics Solutions\Solid Edg\Version109\ and found in the 
<server_name>_Custom_Column_Settings.XML file.


You can set one client to your liking and then push the XML file to all the 
clients to establish the same look & feel for all users. 



Notes and References





Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: XP64
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V109MP3
Function: SEEC

Ref: 001-9028804

KB Article ID# PL8002982

Contents

SummaryDetails

Associated Components