Solid Edge Question about ST10 SEEC installation

2021-10-06T23:51:18Z
DOC_MANAGEMENT

Summary


Details

The Teamcenter integration components for Solid Edge (SEEC) are not on the
ST10 DVDs.


Solution

On the client side there is no longer a seperate install for the Teamcenter
integration component. Install Solid Edge and license the product.

Server side, Solid Edge is now providing SEEC Feature Packages for integrating
with Teamcenter. The SEEC Feature Package is implemented using the Teamcenter
Environment Manager (TEM). See the SEEC_Readme.htm on the Solid Edge DVD for
details.

When installing updates to ST10 the SEEC integration will be updated on the
client when the Solid Edge MP is installed. The SEEC integration update on the
server is delivered in SEEC Feature Packages.


Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V110.0
Function: SEEC

Ref: 001-9024163

KB Article ID# PL8002939

Contents

SummaryDetails

Associated Components

DOC_MANAGEMENT: SEEC