How to place a hole table without a defined origin on the drawing?

2021-10-06T23:51:16Z

Summary


Details

In the previous versions of ST10 it was possible to place a hole table without a defined origin on the drawing by just skipping the "Origin Step" and direcly selecting the holes within the "Select Holes Step".

With the enhancements to the "Hole Table" command in ST10 (e. g. "Selection Method", "Select Features", "Add or Remove Holes Step"), it is no longer possible to skip the "Origin Step". It is now necessary to always define an origin on the drawing.



Solution

However it is possible to work around that situation and achieve the previously known result by the following steps.


  1. Select Home -> Tables -> Hole Table.
  2. Click the elements to define the origin.
  3. Select and accept the geometries for the hole table.
  4. Place the hole table on the drawing.
  5. Create a new layer (e. g. "defined hole table origins").
  6. Select the definitions (e. g. X1 and Y1) of the origin on the drawing.
  7. Move the elements to the previously created new layer.
  8. Activate another layer.
  9. Hide the layer with the origin definitions.

Notes and References

 

Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: SOLID_EDGE
Application: DRAFT
Version: V110.0
Function: TABLES

Ref: 001-9022085

KB Article ID# PL8002923

Contents

SummaryDetails

Associated Components