Teamcenter What specific MP of SE ST8 is supported in TCRS 11.3?

2021-10-06T23:51:13Z
Core Functions

Summary


Details

What specific MP of SE ST8 is supported in TCRS 11.3?

Solution

The latest Teamcenter release supported at the ST8 end of maintenance was: ST8MP12 and Teamcenter 11.2.3. So there is NO ST8MPx will supported in TCRS 11.3.


 
Solid Edge and Teamcenter Integration for Solid Edge compatibility and lifecycle information is maintained here.

Solid Edge End of Maintenance Policy -- SFB-SE-9757
http://uscisgtslrp001.industrysoftware.automation.siemens.com/view.php?sort=desc&p=1&q=SFB-SE-9757&file_type=text&i=sfb-se-9757&k=0&o=0

The latest revision of SFB-SE-9757 for Solid Edge & Teamcenter Integration End of Maintenance has been checked-in and released.

Recommend user for plan to upgrade to Solid Edge with latest released version; for now it's SE-ST10.


Note, Teamcenter delivered a regression in 11.3. Solid Edge ST10 (and ST9MP) require a minimum of 11.3.0.1 (which is covered in the SFB).

Hope this helps.

Notes and References

PD comment.

Hardware/Software Configuration

Platform: INTEL
OS: window
OS Version: 2012
Product: TEAMCENTER
Application: TC_RAPIDSTART
Version: V11.3.0
Function: INTEGRATIONS
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V108MP12
Function: DOC_MANAGEMENT

Ref: 001-9016422

KB Article ID# PL8002886

Contents

SummaryDetails

Associated Components

Core Functions - Client