Simcenter 3D Solutions Export to Adams does not produce an adm file

2021-10-06T23:26:10Z
Simcenter 3D

Summary


Details

How can I export an Adams ADM file from NX Motion? 

Solution

The following Motion Export options are available based on the Simulation 

Solver Options for a Motion Simulation:

1. Simcenter Solver - Export> Mechanism 

2. NX Motion - Export> Mechanism 

3. Recurdyn - Export> Recurdyn Input, ADM, or Mechanism 

4. Adams - Export> Adams Input or Mechanism

To export an Adams ADM file, users need to set the Simulation Solver to 

Recurdyn, which will in turn expose the ADM Translator. 

Notes

KB Article ID# PL8002881

Contents

SummaryDetails

Associated Components

Acoustics Additive Manufacturing Assembly FEM Correlation and Updating Durability Electromagnetics (High Frequency) Electromagnetics (Low Frequency) Flexible Pipe Laminate Composites Margin of Safety Motion Multiphysics NX Open Nonlinear Optimization Pre/Post Response Dynamics Rotor Dynamics Samcef Environment Simulation Process Management Thermal / Flow