Cannot rename wire in Wire Harness using F2 key

2021-10-06T23:51:12Z

Summary


Details

When attempting to rename a wire in the Wire Harness environment the F2 key 
does not work. Not a problem in the Assembly environment.



Solution

The F2 is assigned to 'rename' only in Assembly. To add this to the Wire 
Harness environment:


- close out of Wire Harness 
- select Customize 
- click the Keyboard tab 
- select 'Choose commands from: All Keyboard Assignments 
- scroll down and find Rename in the list 
- in the Usage column change it to "Use in all environments"


If you do not want to use it in all environments, you can enter the Wire 
Harness environment and customize the Keyboard for the specified environment. 


After assigning the F2 key you will need to save the changes as a new theme.



Notes and References





Hardware/Software Configuration

Platform: INTEL
OS: window
OS Version: 764
Product: SOLID_EDGE
Application: APPLICATION
Version: V110MP2
Function: UI

Ref: 001-9014937

KB Article ID# PL8002870

Contents

SummaryDetails

Associated Components