NX Is it Possible to Limit what PMI will be Processed when Running Link to PMI?

2021-10-06T23:26:10Z
NX for Manufacturing

Summary


Details

Is it possible to only select some of the PMI entities that have been created for a part when running Link to PMI?  The intent is to only select the PMI entities that will be checked in a given setup. 

Solution

The Link to PMI button is either all or nothing.  There are no other controls in PMI which could be used to limit which PMI is selected when Link to PMI is run. 

Notes

KB Article ID# PL8002860

Contents

SummaryDetails

Associated Components

Manufacturing CMM