NX Clone import using Part ID Generator but to keep OS filename as item name

2021-10-06T23:26:10Z
NX for Design

Summary


Details

When importing an assembly into Teamcenter, you would like to use option Part ID Generator as Numbering Source to generate the item ID. However, you still want to have OS Filename as item name.
How can this be done ?

Solution

In the native NX part file, you can create a part attribute by the title, DB_PART_NAME, with the value as the OS Filename, then in the import dialog set the Default name as ${DB_PART_NAME}.


To automate the process if you have many files to import, you can also use a journal file to create the attribute for your native NX files.



Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: NXMANAGER
Version: V11.0.2
Function: CLONE_IMPORT

Ref: 001-9010631

KB Article ID# PL8002851

Contents

SummaryDetails

Associated Components

Teamcenter Integration for NX