Tecnomatix Switching from Ribbon UI to toolbar deletes functions.

2021-10-07T00:01:13Z
Process Designer

Summary


Details

Changing from Ribbon User Interface (UI) to toolbar interface leaves little or no functionality in toolbars.  Sometimes pull down menu like "File" are blank.

Solution

This is caused by corruption in temporary layout files.  A workaround to fix this is to remove the folder where they are stored.  Do this when Process Simulate is not running.  When you start Process Simulate again, the program will rebuild the temporary layout.  To find the temporary layout folder to remove  (e.g. "Process Simulate" folder), look in the "C:\Users\%username%\AppData\Local\Tecnomatix" folder.

Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: TECNOMATIX
Application: PLANNING_APPLIC
Version: V13.1.2
Function: ROBCAD_EMS_INTG

Ref: 001-8998116

KB Article ID# PL8002820

Contents

SummaryDetails

Associated Components

Planning Logistics