I have a single node in a group. NX shows the group name in red and has the
text "no displayable entities in group" in the staus window. What does this
message mean?
Solution
In versions prior to NX 11, NX could not display nodes independently of
elements. If a group containing a single node was displayed, then that node as
well as all of the attached elements would be displayed. Starting with NX 11,
there is a switch that allows for the display of a single element. This is
available via the menu - preferences --> model display --> node --> "show and hide
nodes independently" switch. This allows nodes to be displayed directly.
See the following articles in the NX help for a discussion of this in more
detail.
https://docs.plm.automation.siemens.com/tdoc/nx/11.0.2/nx_help/#goto:advanced:p
ref_nodelem_op
https://docs.plm.automation.siemens.com/tdoc/nx/11.0.2/nx_help#uid:xid1128419:i
ndex_advanced:xid389654:xid455577:xid618565
Notes