Solid Edge Cannot activate par, psm amd asm files at the same time with shortcut menu.

2021-10-06T23:51:11Z
ASSEMBLY

Summary


Details

Cannot activate par, psm amd asm files at the same time with shortcut menu in 
the Assembly environment 



Solution

The Activate option has never been in the shortcut menu when parts and 
assemblies are selected at the same time. 
This can be accomplished by selecting the parts and assemblies in the Assembly 
environment and then going to the Select group of commands in the Home, 
Features and other tabs in the Ribbon and clicking the Activate button which 
is located in that group. This simple procedure will Active all parts and 
assemblies that are selected.



Notes and References





Hardware/Software Configuration

Platform: INTEL
OS: window
OS Version: 764SP1
Product: SOLID_EDGE
Application: ASSEMBLY
Version: V109MP10
Function: PATHFINDER

Ref: 001-9008309

KB Article ID# PL8002814

Contents

SummaryDetails

Associated Components

ASSEMBLY: ANNOTATIONS/DIMENSIONS