NX "Select Part" opt isn't available when editing position independent wave feature

2021-10-06T23:26:09Z
NX for Design

Summary


Details

Have a NX part file with a wave feature of the type position independent,
(i.e. the refereced wave geometry does not need to be in the same assembly
structure, nor have the same position as in the original part).
When we do edit on this wave feature there is no "Select Part" option
available in the Part group of the Wave Geometry Linker menu.
How do we get this option so the wave link can be related to another part?


Solution

When you use the wave functionality "position independent" the assemblies
license is not enough as it is with position dependent wave. To create or edit
"position independent" wave features you need a full wave license.

This perticular NX part file have been created with a full wave license
available, but now when it is edited, there is no wave license on the site.


Notes and References


Hardware/Software Configuration

Platform: INTEL
OS: window
OS Version: 764SP1
Product: NX
Application: ASSEMBLIES
Version: V10.0.3
Function: WAVE

Ref: 001-9005339

KB Article ID# PL8002795

Contents

SummaryDetails

Associated Components

Assemblies