Tecnomatix Error: Tecnomatix Application (64bit Release) has stopped working.

2021-10-07T00:01:13Z
Process Designer

Summary


Details

Error:
"Tecnomatix Application (64bit Release) has stopped working.
A problem caused the program to stop working correctly.  
Windows will close the program and notify you if a solution is available".

You see this as soon as the program Process Simulate is executed.

Uninstall and Reinstall does not fix the problem.

Solution

Check the version of NVIDIA driver.  Don't assume the latest version is the correct or best version.
Version 23.21.13.8792 is known to have problems running with Process Simulate.
It causes the program to not run and give you the error listed above.

Version 22.21.13.8541 is older but is known to work with Process Simulate.

Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: TECNOMATIX
Application: PLANNING_APPLIC
Version: V13.1.2
Function: PROCESS_SIMULAT

Ref: 001-9003315

KB Article ID# PL8002781

Contents

SummaryDetails

Associated Components

Planning Logistics