Details
Server status shows a FlexNet Licensing error:-15,10. System Error: 10061
"WinSock: Connection refused".
Solution
Check to see if you have two versions of Solid Edge License Manager installed using Control Panel->Uninstall Prgrams. If so proceed to remove both. Remove the C:\SEFlex folder as well and reinstall the appropriate License Manager for the version of Solid Edge you are running.
Notes and References
Hardware/Software Configuration
Platform: INTEL
OS: window
OS Version: 1064
Product: SOLID_EDGE
Application: SETUP
Version: V110.0
Function: INSTALL
Ref: 001-9004990