Simcenter 3D Solutions Can't use "face of solid" cross section type in a beam collector

2021-10-06T23:26:09Z
Simcenter 3D

Summary


Details

I have created a 1D beam section using the "face of solid" section type, but when I try to edit a beam physical property table, the section is not available.  Also, if I try to create a new section while editing a beam physical property, "face of solid" is not an option.

Solution

"Face of solid" and "General geometry" cross sections can be used for pbeam physical property tables, but not for pbeaml  physical property tables.  Use the physical property type  "pbeam" when the physical table is being created. The property type cannot be edited after the physical property is created.


2017-10-20 09_39_29-Mesh Collector.png 12.99 KB

Notes

KB Article ID# PL8002770

Contents

SummaryDetails

Associated Components

Acoustics Additive Manufacturing Assembly FEM Correlation and Updating Durability Electromagnetics (High Frequency) Electromagnetics (Low Frequency) Flexible Pipe Laminate Composites Margin of Safety Motion Multiphysics NX Open Nonlinear Optimization Pre/Post Response Dynamics Rotor Dynamics Samcef Environment Simulation Process Management Thermal / Flow