NX Using Find Feature to Identify a Sequential Drilling Hole in NX Hole Making

2021-10-06T23:26:09Z
NX for Manufacturing

Summary


Details

Is it necessary for a hole to be identified as a HOLE_ROUND_INTERRUPTED_STRAIGHT when using Find Feature in the Machining Feature Navigator in order to use the Sequential Drilling operation?


InterruptedHole.JPG 64.36 KB

Solution

Sequential Drilling operations do not require that HOLE_ROUND_INTERRUPTED_STRAIGHT be selected when finding this geometry. Features found as a STEPS type hole can also be used to generate interrupted holes.


SeqDrill.PNG 53.23 KB


FBM.JPG 40.06 KB

Notes

KB Article ID# PL8002769

Contents

SummaryDetails

Associated Components

Manufacturing General