Details
How to Increase the Information Windows Text Height in NX11 and Later Releases?
Solution
Since NX11 is now using html format to report all information in the window,
the solution is to press and hold down the "Ctrl" (button on keyboard) while
simultaneously "scrolling Mouse Button Two".
Like all html windows, this will resize the html information windows contents.
Note the altered size is kept from one opened and closed window, to the next opened
information window, within the same NX session.
Notes and References
Hardware/Software Configuration
Platform: INTL64
OS: window
OS Version: 1064
Product: NX
Application: SYSENG
Version: V11.0
Function: UI_TOOLS
Ref: 001-9003708