Details
The Reverse Vector is no longer available when creating Sketch and Sketch in
Task Environment.
Solution
The Sketcher now uses the CSYS Constructor - similar to the Point Constructor
or Plane Constructor. The CSYS Constructor lumps all the direction flipping
into one.
Once you have a preview you can double click on the plane or vector direction
to flip them in the graphics window. If you need detailed control, you can
bring up the constructor dialog, just like in the Point and Plane dialog.
Notes and References
Hardware/Software Configuration
Platform: INTL64
OS: window
OS Version: 764SP1
Product: NX
Application: DESIGN
Version: V11.0.2
Function: FEATURE_MODEL
Ref: 001-9001298