Solid Edge Performance issues working with gage tables defined in Excel

2021-10-06T23:51:04Z
PART/SHEETMETAL

Summary


Details

When working with gage table material properties defined in Excel, there are noticeable performance issues when interacting with the gage tables e.g. slow to open the material properties, selecting Apply, etc.

Solution

This reduced performance when interacting with gage tables that are defined in Excel is occurring because the customer has stored the Excel Gagetable.xlsx file on a network share.

As soon as the Gagetable.xlsx is stored locally the performance interaction issues then no longer exist.

Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: n/a
Product: SOLID_EDGE
Application: PART/SHEETMETAL
Version: V109.0
Function: GAGE

Ref: 001-8971384

KB Article ID# PL8002696

Contents

SummaryDetails

Associated Components

PART/SHEETMETAL: FLAT_PATTERN