Lightweight body visualization behavior

2021-10-06T23:26:08Z

Summary


Details

Get visible lightweight bodies in the modeling workspace. These lightweight 
bodies are representations of solid bodies in the part file. 
If the lightweight bodies are deleted and the part file saved, the lightweight 
bodies will re-occur in the next session. 
Why does these bodies occur and how to get rid of them?



Solution

The reason these lightweight bodies is generated is that the solid bodies they 
represents reside on layer 190. 
Layer 190 is used by NX for the Product Outline functionality in a standard 
installation.


The issue can be solved in 2 different ways: 
- Change the customer default layer for Product Outline. Assemblies -> Site 
Standards, Miscellaneous tab, Product Outlines group, there is the "Layer" 
parameter which controls the layer used for product outline. 
OR
- Move the solid bodies in the model part file to a different layer than 190 



Notes and References





Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 764SP1
Product: NX
Application: ASSEMBLIES
Version: V11.0.2
Function: ASSEMBLY_MODEL

Ref: 001-8992329

KB Article ID# PL8002680

Contents

SummaryDetails

Associated Components