Details
NX 11 on Red Hat 7.x
When launching ugmenu, it manifests in a shell and not the GUI.
Test by launching NX directly - (i.e run ./ugraf or ./ugii)
error while loading shared libraries libXm.so.4: cannot open shared object file: No such file or directory.
Solution
The libXm.so.4 error indicates an OpenMotif issue - probably explaining why there was no GUI when running ugmenu.
The following file is required:
/usr/lib64/libXm.so.4
The missing libXm.so.4 can be found in the RedHat openmotif package .
Obtain and install "openmotif-2.3.3-1.el6.x86_64"
Notes and References
NX Installation Guide for Linux and Mac OS X – page 17 under "Method 1":
The first method uses ugmenu. This is a user menu with an available Motif interface that allows you to select the NX 11.0 product that you wish to run
Hardware/Software Configuration
Platform: INTL64
OS: redhat
OS Version: EL7.0
Product: NX
Application: SYSENG
Version: V11.0
Function: INSTALL_ISSUES
Ref: 001-8938930