Feature Replay in NX11 is slower than Feature Playback in NX10

2021-10-06T23:26:08Z

Summary


Details

When comparing the 'Feature Replay' in NX11 to the 'Feature Playback' in NX10, 
Feature Replay seems slower.



Solution

If using the 'Play' option in Feature Replay, this will make each individual feature current and also regenerate the display at every feature, which will result in a performance difference compared to the 'Continue' <<Play>> option in the NX10 Feature Playback.


However in Feature Replay, if the options 'Start' then 'End' are used instead, this would be equivalent to the 'Continue' <<Play>> option in Feature Playback. This is because the 'End' option does not regenerate the display at every feature. So to achieve similar performance in the NX11 using the 'Feature Replay' command, select 'Start' and then select 'End' as this will update the feature list to the end. 



Notes and References





Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: DESIGN
Version: V11.0
Function: FEATURE_MODEL

Ref: 001-8992702

KB Article ID# PL8002663

Contents

SummaryDetails

Associated Components