After migrating from NX10 to NX11, all users are experiencing up to a 15 second delay when switching from the Modeling application to the Drafting application (and vice versa). The same delay is also happening when switching between drafting sheets.
Solution
- With the cursor on the Desktop background, 'MouseButton3-->NVIDIA Control Panel'.
- Select 'Manage 3D Setting' in the left column.
- On the 'Global Settings' tab, set the Global Presets to '3D App - Visual Simulation'.
- Select the 'Program Settings' tab.
- Toggle 'Select a program to customize:' to 'Siemens NX'.
Hardware/Software Configuration
Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: SYSENG
Version: V11.0
Function: INSTALL_ISSUES
Ref: 001-8991592