How can a Note be created that has a leader from both the left and right sides?
Solution
- Select the 'Note' icon to start the command.
- Expand the 'Leader' group in the dialog.
- In the Leader group, expand the 'Style' and 'List' sub-groups.
- Under the 'List' sub-group, turn off, 'Apply Style Settings to All'.
- Highlight the 'Select Terminating Object' prompt and select the terminating object for the left leader.
- Again, highlight the 'Select Terminating Object' prompt and select the terminating object for the right leader.
Note: Do not place the Note yet. - Under the 'List' sub-group, highlight the leader "ID 1" and toggle the 'Stub Side' option to 'Left'.
- Under the 'List' sub-group, highlight the leader "ID 2" and toggle the 'Stub Side' option to 'Right'.
- Select the 'Specify Origin' prompt and place the Note.
- Close the Note dialog when complete.
Notes and References
Hardware/Software Configuration
Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: DRAFTING
Version: V11.0
Function: ANNOTATION
Ref: 001-8983428