Can NX-Nastran write mass, center of gravity, intertia etc. on result file?
Solution
Yes, these can be outputted into f06 result file if in NX-Nastran Case Control
Section, we include the following parameter:
PARAM,GRDPNT,0
In this case the basic origin will used. If other reference node shall be
used, replace 0 with the node ID.
More about this can be found on or online help:
https://docs.plm.automation.siemens.com/tdoc/nx/11.0.1/nx_help#uid:id485171
https://docs.plm.automation.siemens.com/tdoc/nx/11.0.1/nx_help#uid:id476056::ref42677
Notes