Solid Edge How can I associate view scale with sheet scale property?

2021-10-06T23:50:59Z
DRAFT

Summary


Details

How can I associate view scale with sheet scale property?

Solution

The 'Set Sheet Scale' command can be used for this.


You can use the associative sheet scale mode to derive the sheet scale from the scale of an existing drawing view. This makes the sheet scale associative to the drawing view scale. When you select the Drawing View Scale button on the Set Sheet Scale command bar, you are prompted to select a drawing view with the scale you want to use.

'Set Sheet Scale' command can access by Right mouse button menu appeared once user click the drawing sheet tab.



Hardware/Software Configuration

Platform: INTEL
OS: window
OS Version: n/a
Product: SOLID_EDGE
Application: DRAFT
Version: V109.0
Function: DRAWING_VIEWS

Ref: 001-8957892

KB Article ID# PL8002545

Contents

SummaryDetails

Associated Components

DRAFT: DRAWING_VIEWS