Details
Not getting any gap between three side weld symbol and reference line.
Solution
Gap between three-sided weld symbol and the identification/reference line is adjusted by option 'Three-sided weld symbol offset gap'. If this gap is set to '0' then no gap will be displayed. Adding any suitable positive value will create the gap.
This option is available under Spacing tab of Dimension style.
Notes and References
IR#8967749
Hardware/Software Configuration
Platform: INTEL
OS: window
OS Version: n/a
Product: SOLID_EDGE
Application: DRAFT
Version: V109.0
Function: ANNOTATIONS
Ref: 001-8967749