Details
Customized Print command (added to QAT from "All commands") defaults to Portrait orinetation and seems to be stuck there.
Solution
Go to the Print command from the Application Button and run it there, then the
customized Print command will also default to the Landscape orientation.
Notes and References
Hardware/Software Configuration
Platform: INTEL
OS: window
OS Version: XP32_SP2
Product: SOLID_EDGE
Application: DRAFT
Version: V110.0
Function: FILE
Ref: 001-8981034