NX Opening an Assembly with WAVE data with the message "'Referenced data has been deleted"

2021-10-06T23:26:25Z
NX for Design

Summary


Details

When you open an assembly and the message "'Referenced data has been deleted" is returned.

Solution

This error occurs because a link has been broken. 

A broken link is still a link, therefore can be re-parented so that it becomes active again. A new value has been added to the Link Type option menu in the part's mode Navigator ("Not Broken"), which (in parts mode) displays only the links that are known not to be broken.

Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: ASSEMBLIES
Version: V10.0
Function: PART_FILE_OPS

Ref: 002-8002507

KB Article ID# PL8002507

Contents

SummaryDetails

Associated Components

Assemblies