NX Changing the size of a drawing to the left and down

2021-10-06T23:26:25Z
NX for Design

Summary


Details

Is it possible to edit the size of a drawing so that it can be increased to the left or down?

Solution

No, this is not possible.  The bottom left corner of the drawing is the XY origin and the values of size must be positive.  Any negative value from this origin is not permitted.

Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: DRAFTING
Version: V10.0
Function: DRAWING/VIEW

Ref: 002-8002505

KB Article ID# PL8002505

Contents

SummaryDetails

Associated Components

Drafting