Unable to read the Solid Edge 2019 FlexNet License Server from the Solid Edge client.

2024-10-08T11:49:16Z

Summary


Details

Unable to read the Solid Edge 2019 FlexNet License Server from the Solid Edge Client machine.

There seems to be a firewall blockage problem reading the Solid Edge FlexNet License Manager, this problem still exists even after creating Exceptions for a new inbound rule within the firewall for lmgrd.exe and selmd.exe and rebooting the Server.

Solution

The Windows Firewall offers three firewall profiles: domain, private and public. The domain profile applies to networks where the host system can authenticate to a domain controller. The private profile is a user-assigned profile and is used to designate private or home networks.

In some cases the customer's IT may have to review the Windows Network connection on the Server which is supporting the Solid Edge FlexNet License Manager. Windows will let you set each network you connect to as either a "Private" or "Public" network. By default the customer Network connection may be set to a "Public" option and not a "Private".  To resolve the issue it is suggested that the "Private" option be selected.

On Private networks, Windows enables network discovery features. Other devices can see your Windows computer on the network, allowing for easy file sharing and other networked features. 

On Public networks–like those in coffee shops–you don't want your computer to be seen by others, though, or share your files with them. So Windows turns off these discovery features. It will not appear to other devices on the network and will not try to discover them.

Notes

If you have further inquiries about floating Licensing please refer to the FAQs collection link below:

Solid Edge Floating License FAQs Collection


KB Article ID# PL8002476

Contents

SummaryDetails

Associated Components