NX X
"Open in NX" command does not appear in Active Workspace after upgrading Active Workspace.
2021-10-07T00:08:27Z
NX for DesignNX for ManufacturingAdminNX OpenProduct UsageNX Design TranslatorsCloud Environment
Summary
Details
Problem Description: "Open in NX" command does not appear in Active Workspace after upgrading Active Workspace.
Workaround: Pre-emptive solution: Prior to upgrading Active Workspace, move the file readme_awn0nx.xml from the install directory to the install/readme directory and then perform the upgrade normally.
Post upgrade solution: If the Active Workspace upgrade has already been performed and the symptom listed above is observed, then perform the following actions: · Start TEM · Configuration Manager · Perform maintenance on an existing configuration · Update Database (Full Model – System downtime required) · NX for Active Workspace (awn0nx) · Browse to …\wntx64\install\modules\feature_awn0nx.xml · Next SFB-NX-8002468 Product Information: