Trim curve is not extending

2021-10-06T23:26:24Z

Summary


Details

When trimming a curve, the curve is not extending to the intersection point as expected.

Solution

You need to select a Curve Extension type under the Settings section, and then highlight the Select Region option and select the extended part of the cuve. 




Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: DESIGN
Version: V10.0
Function: CURVE

Ref: 002-8002445

KB Article ID# PL8002445

Contents

SummaryDetails

Associated Components