NX 12 fails to start with the error: "License server version is older that the client"

2021-10-06T23:26:23Z

Summary


Details

NX 12  fails to start with the error: "License server version is older that the client". Older versions of NX start successfully.



Solution

Download and install the latest license server software posted on the GTAC web site at:


  - http://www.siemens.com/gtac
  - Select Download and Upload Files
  - Log with WebKey account user name and password
  - Use the 'Download' tab or the 'Upload ' tab to complete the desired task.
  - Select 'Siemens PLM Licensing' 
  - Select 'Product Updates'
  - Select 'Install'
  - Download and install the desired platform of the SPLM License Server software:

    1. SPLMLicenseServer_v9.0.1_linux_setup.bin - 10,081,600 bytes - Jun 21, 2018 
    2. SPLMLicenseServer_v9.0.1_macos_setup.app.zip - 10,699,137 bytes - Jun 21, 2018 - View Contents 
    3. SPLMLicenseServer_v9.0.1_sol_setup.bin - 9,699,125 bytes - Jun 21, 2018 
    4. SPLMLicenseServer_v9.0.1_win_setup.exe - 22,166,536 bytes - Jun 21, 2018 



Notes and References

N/A

Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 10_1803
Product: NX
Application: SYSENG
Version: V12.0
Function: INSTALL_ISSUES

Ref: 002-8002380

KB Article ID# PL8002380

Contents

SummaryDetails

Associated Components