The customer has problem with editing existing Broken-Out section. When changing the depth of the cutout the Broken-Out view is displayed incorrectly.
This is the customer Broken Out Section :

The user tries to to edit the depth of that the Broken out section:

But when updating the View , the portion of material inside the broken out section will disappear:

Solution
The Broken out section view itself has a defined display depth at the same point as the depth being specified for the Broken out section, so it appears to cut all the way through. Remove or adjust the display depth using the view's context menu to get the desired result.
It is necessary to select the view and MB3 select the option "Set drawing view depth":

Then remove the current depth setting the value as "0" . When updating the the view the result will be correct:

Notes and References
Hardware/Software Configuration
Platform: all
OS: n/a
OS Version: n/a
Product: SOLID_EDGE
Application: DRAFT
Version: V110MP8
Function: DRAWING_VIEWS
Ref: 001-9074106