I want to reorient the text in the cell of a Parts List. In properties if I click on 'Format Cells' – 'Orientation' is greyed out. Why is this?

Solution
The same dialog is used for formatting both Column header cells and Column data cells. However, 'Orientation' can only be changed for the header cells.

It cannot be changed on the data cells. Therefore, the 'Orientation' option in the common dialog is disabled when formatting data cells.
Hardware/Software Configuration
Platform: INTL64
OS: window
OS Version: n/a
Product: SOLID_EDGE
Application: DRAFT
Version: V219.0
Function: TABLES
Ref: 002-8002331