Dear Siemens PLM Customer,
Maintenance Pack 0 for NX 12.0.2 is now available on the Siemens PLM Download Server.
NX 12.0.2 MP0 contains a single fix built for installation on top of the Windows 64-Bit image of NX 12.0.2. The fix addresses the problem where Virtual Reality could not be launched (PR 9208406).
To select the release package for your platform click on the following link or enter the URL in your browser address window:
https://download.industrysoftware.automation.siemens.com/download.php
Note: A valid WebKey account is required.
From the Full Product Download page, Enter "12.0.2.mp00" (including the quotes) in the Search box to see a list of links to the release letter and available release package.
Alternatively, the release package can be found in the file navigator by selecting 'NX' from the menu on the left of the webpage and then navigating through the directory structure by selecting Product updates > Maintenance-packs > Nx12 > Windows (64-bit).
Sincerely,
Siemens Product Lifecycle Management Software Inc.
Digital Factory Division
SFB-NX-8002329
Product Information: