Details
The Where Used dialog is displaying the file on which the process was run, but there are no results displayed underneath the file.
Solution
This problem could occur if there are subfolders in the vault that do not have any permissions defined for the SYSTEM account.
Hardware/Software Configuration
Platform: INTEL
OS: window
OS Version: 764SP1
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V110MP3
Function: BUILT_IN
Ref: 002-8002316