I have a part that I use to create an assembly. I get the following message:

Solution
As stated in the error message - one reason could be that the part has been divided. To determine this and resolve the issue activate the 'Divide part' command. As this is no longer on the main menu it is best accessed by using the Command Finder tool.

Select any line in the Divide part window and click 'Remove'.

All entries should be cleared.

Once done, the part can be used in an assembly without further problems.
Hardware/Software Configuration
Platform: INTL64
OS: window
OS Version: n/a
Product: SOLID_EDGE
Application: ASSEMBLY
Version: V219.0
Function: COMPONENTS
Ref: 002-8002261