In this example the user is working in a SEEC managed environment. When they do a Mirror operation they get the following message:
![](/kbassets/PL8002256/c066504c432b4bf9c76b033a9e24b256434815cd0fdc99b83db74de92073.jpg)
Solution
The reason for this is that the entire folder structure for the Solid Edge templates has not been imported - only a selection e.g. ISO templates were imported. This is known to adversely impact downstream processes such as Mirror and Divide Part.
The solution is to import the entire folder structure for the templates into Teamcenter.
Hardware/Software Configuration
Platform: INTL64
OS: window
OS Version: n/a
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V110.0
Function: SEEC
Ref: 002-8002256