Since ST10, when creating a Hole table the user is obliged to define an X and Y origin for the holes, which was not the case in previous versions.


Some users would prefer that this does not appear - is there a way to not display this?
Solution
The easiest solution is to move the X/Y origin elements to another layer and then hide the layer.
- First create a new layer and give it a meaningful name e.g. hole table origins.

- Then select the X/Y hole origin elements in the drawing view.
- On the layers tab click the 'Move Elements' button.

- You will be prompted to select the layer to move the elements to - in this case 'hole table origins'.

- As this will make 'hole table origins' the active layer you will need to make another layer active e.g. Default.
- Then you can select the 'hole table origins' layer and RMB - Hide.

- The XY hole table origin elements will no longer be visible.

Hardware/Software Configuration
Platform: INTL64
OS: window
OS Version: n/a
Product: SOLID_EDGE
Application: DRAFT
Version: V110MP8
Function: TABLES
Ref: 002-8002225