Solid Edge What controls the setting for the default Revision Rule for Solid Edge/SEEC

2021-10-06T23:52:38Z
DOC_MANAGEMENT

Summary


Details

Which setting or preference controls the default Revision Rule for Solid Edge/SEEC.

Solution

This is controlled by the Teamcenter preference "Tc_config_rule_name".  The preference is read by Solid Edge/SEEC the first time the connection is made to the Teamcenter server.  At that time the value is written to the registry and is controlled by that registry setting from that point forward.  When you want to change the value, it can be done on the Solid Edge/SEEC File Open dialog. 

Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 764SP1
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V110MP8
Function: SEEC

Ref: 002-8002183

KB Article ID# PL8002183

Contents

SummaryDetails

Associated Components

DOC_MANAGEMENT: SEEC