Error message returned during Initization of Insight services

2021-10-06T23:52:50Z

Summary


Details

The following error message was returned when the Sharepoint Farm administrator attempted to run the Initialize Insight Services after the password for the Sharepoint Farm administrator was changed.

"The operation returned HTTP Error 401. This can happen when the IIS web site uses Integrated Authentication as described by Microsoft Support in Knowledge Base Article ID: 896861.  Consider the details in this article and then retry the operation."

Solution

The administrator must reset the Sharepoint Farm administrator password in Central Administration.  With several locations existing where this needs to be done, it is easier to use the following cmdlet in Sharepoint Management Shell:

"set-SPManagedAccount –UseExistingPassword -Identity [Sharepoint login]".

The administrator will be prompted to enter the new password.  After this he will be prompted for a confirmation.  Enter "A" for Yes to all.

After the process completes the administrator needs to run "iisreset" in the same Sharepoint Management Shell window.

The Initialize Insight Services should run successfully.

Hardware/Software Configuration

Platform: INTEL
OS: window
OS Version: 2012_R2
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V219.0
Function: INSIGHT

Ref: 002-8002398

KB Article ID# PL8002398

Contents

SummaryDetails

Associated Components