A customer wants to open every Solid Edge assembly structure as "Read-only" by default when using SEEC. How to configure this for every user? Is there a Teamcenter preference or setting?
Solution
There is no Teamcenter preference or setting to force this for every user, however each user can set this option during the File -> Open action in the dialogue. When using the "Read-only" option with "All Levels" any edit or open action from the path finder will open in Read-only mode and a manual "Check-out" would then be required before you can upload any changes.

When in this dialogue use the "Save as Default" option, then every new File -> Open action will use the new default settings.

Hardware/Software Configuration
Platform: INTEL
OS: window
OS Version: n/a
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V100.0
Function: DOC_MANAGEMENT
Ref: 001-8374956